Hello Support team,
I receive some questions from customer for TPS65987D usage.
*They plan to support up to 60W and <3A, they don't need to support e-marker. In this case, PP_CABLE pin can connect to GND as unused pin, is thier understanding correct?
*Datasheet page 25, PPHV1 recommend to use as sink and PPHV2 as source. In case of power bank, can TPS65987D accept PPHV1 only as sink and source path? TIDA-01627 set PPHV2 pulled GND. Or should they use both PPHV1 and PPHV2? In this case, please advise how to connect each pin.
* About dead battery configurations, if BP_NoResponse is selected and battery voltage is lower than 3.3V, TPS65987D can't enable internal SW and system never start up. Is their understanding correct? If you have general usage for dead battery on power bank, please introduce it. "dead battery configurations" recommendation or external 3.3V design (ORing power source from battery and VBUS) would be helpful.
Thanks,
Koji Ikeda