Other Parts Discussed in Thread: SN65HVD11,
Hi,
I am planning to use SN65HVD75DRBT in my design.The R,D,RE,DE signals are from external chip and those are 5V level. I see in the SN65HVD75DRBT datasheet claiming "5-V Tolerant Logic Inputs Compatible With 5-V Controllers". But the Recommended Operating Conditions suggests the high level input shall be maximum VCC, which is 3.3V in my design. Can you confirm that I can provide 5V inputs to SN65HVD75DRBT chip without affecting device reliability and 5 years of product life?
thanks, Shanoj