Other Parts Discussed in Thread: TCAN332, SN65HVD232, TCAN1042-Q1
Related to question asked by Shu-Cheng LIN on TCAN332 ESD/Surge protection (quoted below)
the TVS recommended for most CAN/CAN FD transceivers have Vbreakdown of 24-36V. This works for most transceivers as their CANH and CANL have Vmax/min of 40V/-40V.
For a CAN/CAN FD transceiver with CANH and CANL Vmax/min of 14V/-14V like the TCAN332, what is the recommended TVS protection device?
(I am sure the part recommended should be a "bi-directional" part but another pertinent issue is which part also have a Vbreakdown (breakdown voltage) that is NOT so high that by the time it starts working,
the TCAN332 would have been spoilt.
Mr. Lin's original query quoted below for everyone's easy reference:
TCAN332 specification 8.1 mentions that the maximum can withstand -14~+14V, then should I choose 14V two-way TVS?