Other Parts Discussed in Thread: SN75176B, THVD1450, THVD1500, THVD1550
Hi TI
1. If SN65176B chip pin1, pin4 serial port RX, TX signal is 3.3V level, can it be directly connected to SN65176B chip without level conversion?
According to specifications, D, DE, / RE signals larger than 2V are high levels.
2. What is the A/B foot current of SN65176B chip? There are two references to current in the specifications.
What would the current be if 256 loads were fully loaded according to RS485 protocol?
Thank you
Jerry