Hi team,
We will use DP83TC811SEVM for the study of in-vehicle Ethernet.
I want to confirm the establishment of communications and obtain EMC reference data before making my own board.
With this evaluation board, the link status can be monitored with LED.
However, if the link error is instantaneous, it cannot be monitored by the LED.
Can this be latched to drive the LED?
I want to check if there was an error without reading the register.
I'd like to do an EMC test.
Can the T1 phy run standalone without a PC connection?
I understand that EVM is not for EMC testing.
If you can share test data such as emissions and BCI, I would appreciate it if you could share the board layout and results.
Best regards,
Tomoaki Yoshida