Hi Team,
Could you please help to figure out the max-rating of DP83848's TD+/- and RD+/-(max voltage that won't do damage to the device)? Thanks.
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you please help to figure out the max-rating of DP83848's TD+/- and RD+/-(max voltage that won't do damage to the device)? Thanks.
Best Regards
Hi Wade,
Does the "-0.5V to Vcc+0.5V" mean the differential voltage or the absolute value? We are using the differential output, the P pin voltage is tested to be 4.7V and the N pin voltage is tested to be 3.3V(Vcc pull-up voltage). If it's the differential voltage, what is the absolute voltage value? Thanks a lot.
Best Regards,
Qiang
Hi Wade,
Could you please update the answers? Thanks a lot!
Best Regards
Hi Wade,
Could you please update the feedback? If it is the single-ended voltage, I think it's too low... Because in the actual application, the single-ended voltage can easily exceed the Vcc+0.5V..
Best Regards
Qiang,
I just received feedback from the team.
The absolute max ratings for the MDI pins (TD-, TD+, RD+, RD-) is 5.5V.
I apologize for delay.
If this answers your question, please click "This Resolved My Issue"
Regards,
Wade
Hi Wade,
Thanks for your reply. There are 2 points to check with you:
Best Regards,
Qiang
Qiang,
WVB: This specification is not currently in the DS. I am requesting that this information get added. I am researching to see if there are equivalent circuits for the MDI pins that can be provided.
WVB: Unfortunately, this is not something that can be characterized sufficiently. This would apply to the Absolute Max Ratings section with following note:
(1) Stresses beyond those listed under Absolute Maximum Ratings may cause permanent damage to the device. These are stress ratings only, which do not imply functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.
I am out of the office until Tuesday. I will let you know if there is a equivalent circuit.
Regards,
Wade
Qiang,
I was not able to locate equivalent circuits.
I have informed the mass market team that the abs max value is missing. This should be put into queue to get updated on next datasheet release.
Regards,
Wade