Other Parts Discussed in Thread: UCD9248, UCD9240
Hi team,
Customer is wondering is that possible for 811S-Q1 to enter sleep mode while link down? Or it must be in link up state to enter sleep mode?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Customer is wondering is that possible for 811S-Q1 to enter sleep mode while link down? Or it must be in link up state to enter sleep mode?
Thanks
Hello Fery,
"Once in sleep mode, all PHY blocks are disabled except for energy detection on the MDI. All register configurations are lost in sleep mode. No link can be established, data cannot be transmitted or received and SMI access is not available when in sleep mode"
This is from section "8.4.8 Sleep" of the datasheet.
Thanks,
Vibhu
Hello Fery,I want to ask you some questions about UCD9248
1.For myown board designed with reference to KC705 ,firstly, I download the .xml files of ucd9248 from www.xilinx.com/.../56811.html. when I load the .xml file to the devices , the following error occurred:
14:57:14.218 CUSTOMER ERROR Summary READ_VOUT on rail #1 (0.003 V) was not within 3% of VOUT_COMMAND (1.000 V)
14:57:14.239 CUSTOMER_LOGONLY ERROR Summary READ_VOUT on rail #1 (0.003 V) was not within 3% of VOUT_COMMAND (1.000 V) at TIDP.Factory.TaskLibrary.UCD9240.Validate_Vout_Device_Reading(Int32 rail_num, Double percent_pass) in c:\Anne_TI\Workspaces\FusionTools-Main\Libraries\TIDP\TIDP.Factory.TaskLibrary\UCD9240.cs:line 548 at TIDP.Factory.TaskLibrary.UCD9240.Validate_Vout_Device_All_Rails(Double percent_pass) in c:\Anne_TI\Workspaces\FusionTools-Main\Libraries\TIDP\TIDP.Factory.TaskLibrary\UCD9240.cs:line 596
2.For the KC705, fusion_digital_power_designer cannot find devices.I cannot see any information of rails.,
Hi Vibhu,
My questions is, whether we can enter sleep mode during link down?
Hello,
Please post the question regarding UCD9248 in the "Power management forum", a specialized engineer can you assist you there.
Thanks,
Vibhu
Hello Fery,
Can you please give us more details about your application? Why are you trying to enter sleep mode during link down?
Thanks,
Vibhu
Hello Ferry,
If this is still an issue can you please give me more information about the use case and application? Why are you trying to enter sleep mode during link down?
Thanks,
Vibhu