Hi All:
I am wondering if it is possible to add the 2ns skew via the PHY in my case. Or I have to figure something else to add the skew
Thanks,
CK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All:
I am wondering if it is possible to add the 2ns skew via the PHY in my case. Or I have to figure something else to add the skew
Thanks,
CK
Hello CK,
Assuming that you are operating in the 1000M RGMII mode, there is a way to configure transmit/receive delay.
Please refer to section "9.4.4.2 1000-Mbps Mode Timing" of the datasheet (http://www.ti.com/lit/ds/symlink/dp83869hm.pdf) for more information on enabling and configuring this delay.
Thanks,
Vibhu