Hi team,
I have a question about TCA9555 bus address setting. 1.8V is applied for Vcc pin and A0~A2 pin. 10 kohm is used on pull-up to 1.8V and pull- down to GND.
However, the pull-up voltage is 0.35V only. Do I need resistor for pull-up /down? or tie VCC and GND directly?
1.Want to know is there internal pull high or pull low resistor in TCA9555PWR pin:21?
2.Is this any problem to have 10K ohm pull high resistor connect to pin:21
3.Do you have any suggestion for this pull high resistor value R163?