I have this part designed in on a very large board 22" x 26"
There are several USB 3.1 Gen 2 sources on the board, at different distances from the edge of the board where the connectors are. Each of them has a TUSB1002, to help drive the long traces.
The ones closer to the edge of board work, the ones further away do not.
In order to figure out the proper equalization settings for the TUSB1002, I have created a breakout board, to allow me to bring a signal source into the board to test the S-parameters and create an EYE diagram
To characterize the circuit (PCB traces + TUSB1002 + Connector) I am using a PNA: Keithley N5222B.
THE PROBLEM: when the TUSB is in the circuit, stimulated by the PNA, I am getting no signal at the output of the TUSB1002 (power is ON, and the input EN pin is left floating). When I removed the TUSB1002 from the circuit and bypassed it, I DO get signal, which proves that my cables/connections/traces are OK
QUESTION 1: Is there an issue with using a PNA to characterize the TUSB?
QUESTION 2: How did TI generate the SDD21 plots in the datasheet? Can you share with me what instrument was used for characterization?