Hi, Is it possible to use SN65LVDS93A-Q1 with other supplier's LVDS Ser Des such as BU90R104 as Ser Des combination?
ito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Is it possible to use SN65LVDS93A-Q1 with other supplier's LVDS Ser Des such as BU90R104 as Ser Des combination?
ito
Hello Ito,
From the high level there should be no problem to do this but we have not done a deep technical analysis on the other supplier's device in order to understand if all timing margins and DC electrical levels can be met when interfacing these two devices. The customer can reference our DC and AC electrical datasheet parameters for SN65LVDS93A-Q1's output LVDS signals and compare against the other supplier's LVDS input signal characteristics. If these match correctly then the pair should operate together.
Best Regards,
Casey
hI Casey
by the way, What is typical cable length for SN65LVDS93A and SN65LVDS94?
Hello Ito,
We do not have detailed cable length information for these devices but typical applications utilize FPC cable which is usually somewhere between ~0.05m - 0.6m
Best Regards,
Casey