This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987EVM: TPS65987EVM

Part Number: TPS65987EVM

Hello,

I try to use the GUI tools and the TPS65987EVM for a new prodruct developpement

on the USB-C I always connect a Galaxy S40 smartphone ;

The TPS65987EVM SYS_PWR is connected to a power supply 5V 2A

The goal is when the power supplys is on the Galaxy S40 must be charged (sink mode) , when the power supply swithc off  the S40 must swap to source to power up the board.

Could you welp me to set up the  TPS65987, because since now I was not able to manage this.

Also do you have any documentation about the regiser and command of the TPS65987.

Best regards

David LAURENT