This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25740B: Need confirmation on the design and layout

Part Number: TPS25740B

Hi

Please find attached the schematic and layout file for the USB PD circuit (2 ports) based on TPS25740B.

This design has option to bypass the DC/DC converter

to source 20V straight to the USB PD through the controller.

For the remaining voltages 5V, 9V, 15V we have a DC/DC converter (LM73606RNPR).

Kindly review the DC/DC converter circuit and layout also.USB_PD_Review_29Jan2020_6.zipUSB_Type-C_ckt4.pdf

Regards,

Felix.