Part Number: TPS65987EVM
Hi Interface Team!
I have received a question from a customer working with the TPS65987EVM in sink mode.
This is from the customer:
I have used the TI Application Configuration Tool to create a project with 4 fixed sink PDOs.
The binary created from this project works, and I can successfully negotiate all of the contracts.
However, I tried to reduce the number of PDOs by creating a variable sink PDO of up to 20V at 4A, and this failed to negotiate anything over 5V at 3A.
What is the purpose of the variable sink, and can I use a single variable sink to test all 4 PD contracts?
Let me know if you need any more information!
Thank you,
Mitchell