This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TDP158: voltage range of SDA_SRC

Expert 3445 points

Replies: 2

Views: 73

Part Number: TDP158

Dear team,

Is there any rick if I follow SDA/SCL_SRC design with TDP158EVM?

There is a pull up resister to BOARD_5V at SDA/SCL_SRC bus. But the absolute maximum voltage of this two pins are only up to 4V in our datasheet.

Did I need level shift IC to meet datasheet recommend or just  follow  EVM schematic is good?

Thanks.

Ben

  • Ben

    This is a mistake in the schematic, they should be pulled up to BOARD_3P3V, not BOARD_5V.

    Thanks

    David

  • In reply to David (ASIC) Liu:

    Hi David,

    Thanks for your information.

    Please help to correct schematic design. :)

    Ben

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.