Other Parts Discussed in Thread: CONTROLSUITE, TLK110, , TLK105, TLK106
Hello,
Using the lwip control suite example found here:
C:\ti\controlSUITE\device_support\f28m36x\v220\F28M36x_examples_Master\enet_lwip\m3
We have a custom board using the F28M36 chip with the DP83822H. The example seems to have been written for a board with the TLK110
Looking to modify the existing example to work with the new PHY. As far as I can tell the Pins are setup on the same pins, and the PHY Addresses used are shared between the two PHYs. The below signals were captured with a Saleae logic analyzer, and I am uncertain what to make of the MDIO analog reading where the high/low during the data portion are changing state but not reaching full low.
Any information that would be helpful for migrating to the DP83822H to help successfully test this hardware?