This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Configuring EVM to tap into I2C bus of customers design?

Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP, USB2ANY

Hello Team,

How can i configure the ds90ub954 evm so that i can use the TI GUI/Analog launchpad to tap into the I2C bus of the x954 on customers hardware and try to configure the des and camera?

  • Hello Julio,

    If you hold the 954 in reset by pulling the PDB pin low on the EVM, then you can jumper the I2C lines from the EVM to the customer board and the GUI will think that the 954 on the customer board is the 954 on the EVM. Alternatively you can use a USB2ANY module instead of a 954 EVM. The USB2ANY or Aardvark also work with ALP. 

    Best Regards,

    Casey