This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 8
Views: 134
Part Number: TPS65987EVM
Hi Team,My customer is evaluating PD behavior with TPS65987EVM.He set TPS65987EVM source only and tests charge operation to connect to note PC that supports USB PD. However the result is different between long cable and short cable as the following.--------------------------------100cm USB Type-C cable: TPS65987EVM can charge note PC (no ploblem)50cm USB Type-C cable: TPS65987EVM cannot charge note PC--------------------------------It seems PD negotiation is failed when using short (50cm) cable..Do you have heard same issue?Best Regards,Yaita
Hi Yaita,
According to your description, it seems that the issue is from 50cm cable. Can you confirm that the 50cm cable is good ?you can try to use the 50cm cable with TPS65987EVM to charge a type-c mobile phone, or use two TPS65987EVM (one DFP, one UFP ) to verify whether this cable is OK.
Best Regards,
Kevin
In reply to Kevin-Cheng:
Hi Kevin-san,Thank you for your reply.My customer tested with two 50cm USB Type-C cable (ELECOM, generic), the result is the same. TPS65987EVM cannot charge note PC.He also tested with AC adapters (Anker, ELECOM) which is on the market instead of TPS65987EVM, these can charge note PC (no ploblem) even if 50 cm cable is used. Do you have an idea how to improve the situation?Best Regards,Yaita
In reply to K.Yaita:
Can you help get the PD log of the two situation :
1. 50cm cable with TPS65987EVM charge note PC
2. 50cm cable with AC adapter charge note PC
And also, Let them use GUI debug mode to get the PD state machine trace of below two situation:
2. 1m cable with TPS65987EVM charge note PC
Best regards,
Hi,
I also face type-C similar issues in USB Cameras during enumeration. Some manufacturer cables work fine other manufacturer cables not working issue. This might be because of connection issue. Can you please try to connect two orientations in the EVM and confirm?
Thanks.
Vignesh.M
is there any update about this case, if not, i will close this track.
Hi Kevin-san,Under the influence of COVID-19, I heard my customer is retricted to go to the office.I heard he can get PD log and state machine trace sometimes this week.I will update when I get the result.Best Regards,Yaita
Since I have not received your reply for several days, I will turn off this item. If you have further question, you can reply it again.
If this answers your question, Please click "This resolved my issue" button.
Hi Kevin-san,I apologize for delay.. I heard there is something wrong with his EVM now and he hasn't connect with PC so he is looking into it.Please let me contact you again if we have update.Thank you for your cooperation.Best Regards,Yaita