Hi team,
Can you recommend a device which does USB to UART translate and simpler?
Customer is considering below device and we need a part to replace it.
Thanks!
George
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can you recommend a device which does USB to UART translate and simpler?
Customer is considering below device and we need a part to replace it.
Thanks!
George
we have TUSB3410 which is similar with HT42B564-x 16NSOP
Hello Brian,
Does this device supports virtual keyboard function without the need of driver?
Thanks,
George
Hi George,
TUB3410 is the product to use for USB to UART however our VCP driver is required for USB to UART operation. THe main difference here is that TUSB3410 will be configured as a COM port whereas the HT42B564 seems to be configuring as a HID class device.
TUSB3410 can also be configured as a HID class device but for USB to I2C function. TUSB3410 will be configured as a USB HID device which does not require additional driver however some software will need to be developed to control TUSB3410 using standard HID calls. We do have a API and example code for this that can be provided.
Hi Malik,
Yes customer need to configure the device to HID device. Can you share the API and the example? Thank you very much!
Geroge
Hi George,
Please accept my friend request so that I can send you the software through E2E DM. Please post on your original thread once you have done so.