I did erroneously design this chip in, on just received very expensive and complex prototype boards, so that VccA is powered at 3.3V and VccB at 1.8V.
I now need fixing those boards with as little noticeable intervention as possible.
The easier way i see is soldering the chip 180° rotated, than rearranging only GND and OE connections.
But doing that way SDA and SCL lines are swapped with respect to pin names of TCA9406.
As far as i know this should not be a problem, both lines expect the same electrical behaviour in I2C standard.
Q1: So why did TI name these pins definitely? is there anything else inside it's logic forbidding or geopardizing this functional pin swap? the datasheet doesn't mention any as far as i can see.
Q2: Is there (, for magic!,) any known alternate part coming in R-PDSO-G8 package with same pinout but able to perform I2C 400 Khz level translation from 3.3V on side A to 1.8V on side B?
Thanks
Francesco