Other Parts Discussed in Thread: TCA9517-Q1, TCA9306-Q1, TCA9517, TCA9617B, PCA9306, TCA9511A, TCA9803
Hi,
I would like to ask you a question about "level sifting".
My customer is planning to use I2C I/F with "CPLD" (master) as below.
CPLD(master) --- P82B96 --- EEPROM(slave)
But the I/F level between master and P82B96 is difference, master "L" is 0.8V(typ) and P82B96 is "0.88(typ) and 1.0V(max)".
So to solve this situation, the customer is considering to use TCA9517-Q1 or TCA9306-Q1 as "level shifter".
That is to say,
CPLD(master) --- TCA9517(or 9306) --- P82B96 --- EEPROM
CPLD --- TCA9517 : 3.3V or 1.8V
TCA9517 --- P82B96 : 5V
TCA9517 will be used as "level shifter" in this case.
I would like to ask you, is it possible this kind of usage, right?
Thank you very much for your support.
Best Regards,