Hi,
Can the PCA9306 only do voltage translation between the standard voltages mentioned in the datasheet? I need the translation to happen between 3.3 and 4.6V. Is it possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can the PCA9306 only do voltage translation between the standard voltages mentioned in the datasheet? I need the translation to happen between 3.3 and 4.6V. Is it possible?
Hi Karthik,
Yes - it's an analog device and is able to operate at any voltage level below the recommended maximum of 5.5 V. The discrete voltages listed in the datasheet are just for reference since these are commonly-used values.
Regards,
Max