This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD82: Please Recommend Suitable part with lowest cost

Part Number: SN65HVD82
Other Parts Discussed in Thread: THVD1500

Dear Team,

Customer have below requirements for RS485, please recommend suitable part with the lowest cost:

All serial ports shall be able to handle the following communication speeds with a maximum deviation in transmitting and receiving speed(s) of ±3 %:

- 300 bps

- 1.2 kbps

- 2.4 kbps

- 4.8 kbps

- 9.6 kbps

- 19.2 kbps

- 38.4 kbps

- 57.6 kbps

- 115.2 kbps

- 230.4 kbps

 

All serial port shall have at least a 16-byte FIFO.

 

The RS485 bus transceiver shall be of type “Slew-Rate limited”.

 

The serial port shall support RS485 Modbus and pro-vide the power output of +12V, 200mA from each port.

Note: RS485 is a balanced signal point-to-multi-point layer 1 interface according to /ISOIEC8482/ and /TIA-EIA/

 

Serial port transceivers must have upper slew rate limit above or equal to 230.4 Kbit and below or equal to 2 * 230.4 Kbit.

 

There shall be a SW selectable line to line termination/bias for RS485 with 330-ohm termination and 680ohm pull-up to +3.3V & 680ohm pull-down to 0 V.

 

The RJ45 connector pinning shall be as specified in below table.  Pin1 & Pin3 is same A, Pin2 & Pin6 is same B

The ports must be isolated to each other and polarity protection must be ensured.

 

BR

Kevin