Hello,
We have 2 problems
1. We've had some confusion on the TUSB321 VBUS_DET pin and the voltage thresholds discussed in the datasheet. In some places (ie 6.1 Absolute Maximum Ratings) VBUS_DET allows from -0.3 to 4.0V. Other places (ie 6.3 Recommended Operating Conditions) where the VBUS_DET threshold voltage is described as 4.0V, which indicates to me that the voltage needs to exceed 4.0V in order to be detected). There appears to be 2 different definitions for VBUS_DET, where one means the pin itself, and the other means the "5- to 28-V VBUS input voltage" on the other side of the RVBUS (909k resistor)
2. I cannot find any indication for how the DIR logic works in conjunction with TVBUS_DB. I think that the CC1 and CC2 pins are "polled" just after TVBUS_DB times out, which would indicate that if VBUS_DET was not connected, or did not change, then no changes on CC1 and CC2 would be detected, and no change would happen on the DIR pin.