This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Connection with RJ45

Part Number: DP83867IR

Hi,

My customer would like to know below connection between DP83867 and RJ45 terminal.

DP83867 PIN RJ45      

TD_P_A

6

TD_M_A

3

TD_P_B

2

TD_M_B

1

TD_P_C

8

TD_M_C

7

TD_P_D

5

TD_P_D

4

Is it possible to connect above connection?

The connection between EtherPHY and RJ45 Usually connect as below,:

However, DP83867 EVM connection are below:

In EVM, the order of PIN number of RJ45 is opposite from normal connection. For example, PIN 1 of RJ45 connects to TD_D_N but the PIN1 connect to TD_P_A. It looks like DP83867 can automatically detect and connect for both case, then, customer would like to know if the device can automatically detect and connect his own connection.

Regards,
Nagata.