Our board has no connection to the RX_CLK pin. The OPCODE config pins set the opcode mode to 1. After re configuring to 1000BASE media converter mode, our board behaves as if link loss pass through is enabled. Disconnecting either port brings the other port down. However, the register setting for register 0x1EC appears to indicate that link loss pass through is disabled.
I changed bit '0' of register 0x1EC on and off but this didn't affect the behavior of the board.
Here is register dump:
0x000: 0x1140 0x7969 0x2000 0xa0f1 0x0001 0xcde1 0x006f 0x2001
0x008: 0x4006 0x0200 0x3800 ...... ...... 0x401f 0x616d 0xf000
0x010: 0x5048 0xbf02 0x0000 0x5c40 0x29c7 0x0000 0x0000 0x0040
0x018: 0x615b 0x4004 0x0002 ...... ...... ...... 0x0012 0x0000
0x020: ...... ...... ...... ...... ...... 0x0480 ...... ......
0x028: ...... ...... ...... ...... 0x141f 0x0000 0x0221 ......
0x030: ...... 0x10b0 0x00d0 0x0000 ...... ...... ...... 0x0003
0x038: ...... 0x0000 0x0000 ...... ...... ...... ...... ......
0x040: ...... ...... ...... 0x07a0 ...... ...... ...... ......
0x048: ...... ...... ...... ...... ...... ...... ...... 0x0166
0x068: ...... ...... ...... ...... ...... ...... 0x021c ......
0x080: ...... ...... ...... ...... ...... ...... 0x0077 ......
0x130: ...... ...... ...... ...... 0x1000 0x0000 ...... ......
0x170: 0x0c0f ...... ...... ...... ...... ...... ...... ......
0x180: ...... ...... ...... ...... ...... ...... ...... ......
0x188: ...... ...... ...... ...... ...... ...... ...... ......
0x190: 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000
0x198: 0x0000 0x0000 ...... ...... ...... ...... ...... ......
0x1a0: ...... ...... ...... ...... 0x0000 0x0000 0x0000 ......
0x1d8: ...... ...... ...... ...... ...... ...... ...... 0x0044
0x1e0: 0x417a ...... ...... ...... ...... ...... ...... ......
0x1e8: ...... ...... ...... ...... 0x1ffd ...... ...... ......
0xc00: 0x1140 0x616d 0x2000 0xa0f1 0x0020 0x4060 0x0007 0x2001
0xc08: 0x0000 ...... ...... ...... ...... ...... ...... ......
0xc10: ...... ...... ...... ...... ...... ...... ...... ......
0xc18: 0x01ff 0x0011 ...... ...... ...... ...... ...... ......
Is there another register value that needs to change to disable link loss pass through?