Other Parts Discussed in Thread: DP83869, DP83869EVM
Hello,
we want to use DP83869 as a media converter in connection to a SerDes IC, with FX-side towards to SerDes. I have measured a phase difference between 25MHz tact input (pin 19 DP83869) and 125Mbps data-output (pins 14-15) on eval-board and it seems to be variuos by every single power-up.
So if I started DP83869 once, the delay between rise signal edges XI to SO_N/SO_P is constantly and will not change. But after the next power-up it will have another fix value and there is no regularity of changing it by every power-up. I come to conclusion, that the data output (pins 14-15) sets randomly to a clock input by different power-ups.
Is this assumption correct? Could we control a time offset between tact signal and data output by any means of DP83869?
With best regards,
Arsenii Maksimov