TUSB1211: USB-OTG connections

Genius 15905 points

Replies: 1

Views: 14

Part Number: TUSB1211

Team, 

Can you please direct me to some details on how to connect TUSB1211A1ZRQ and TM4C129ENCPDT signals related to USB-OTG operation.  Specifically both the processor and the transceiver have connections for the ID and the VBUS inputs from the USB connector, how should those connections be treated? Should I only connect the identified signals to the processor, only connect the identified signals to the transceiver, or maybe mux the signals to both devices?

There is a schematic that shows the connections being made to the transceiver in the datasheet, but if that is the case, then are the ID and VBUS lines on the processor recoverable for other uses?  

Thanks

Viktorija

1 Reply