Hi,
I would like to configure certain Product Type VDO's and I see that register 0x47 allows me to do that. By the PD spec I'm able to configure the "ID Header VDO" "Cert Stat VDO" and "Product VDO"(Assuming VDM header is automatically created). The problem is when I try to define the first "Product Type VDO" the Application Configuration Tool defaults to "AMA Product Type" and I'm not able to create a different type of entry. Not that if I set "Number of Identity objects" to 6 the, 5th and 6th objects allows me to simply define a 32bit value(anything I want).
"Number of Identity Objects" = 4:
"Number of Identity Objects" = 6:
It seems one Product Type VDO is forced to be AMA type. Spec doesn't seem to indicate any such restriction:
Thanks,
Ilya