Hi,
I connected the USB-C-PD-DUO source to the sink. I was able to change the VBUS from 5V to 9V and 15V, however when I attempted 20V following the instructions according to the EVM user guide, I was unable to get a 20V VBUS. Both of the boards were tested from out the box configuration and were reflashed once. In both cases, I was unable to get the 20V VBUS and the 5V LED lit up.Based off the scope, when the 20V is pressed the VBUS voltage goes up to 18V for a second then drops to 5V. What I do to make it hold a 20V VBUS. I have included the set-up and state of the EVM when the 20V was pressed.
Best Regards,
Zhen Kit