Hi teams
We plan to debug the external framesync sensor which used the 953 Serializer.
the serializer 953 hardware design as below:
TI_F_SYNC source is coming from DS90UB960.
I want to know.if the gpios of 960 did not connect any external source.The 960 can be output clock from internal?
Our current design as below:
If it still can work for 953,if 960's gpio did not use external clk source,it only use 960 internal PLL clk.
or use a external clock source ,it should be What frequency
BRs
thanks