hi teams
This is the question I submitted before. I used the internal trigger sensor. The problem has been solved, and 4 cameras can be turned on at the same time, and preview normally.
Now I have replaced it with the external trigger camera. I use the internally generated framesync mode to provide framesync signals to the sensors,The following is the configuration of the register. And the display effect is shown in the picture.
There are three camera images that can be previewed in real time, but the images are misplaced, as shown in the picture. The other one camera only shows one image and cannot be previewed in real time
Is this a problem with sensor or 960 or 953 configuration?
Looking forward to your reply, Thanks very much.
i2cset -f -y 8 0x3d 0x4c 0x01
i2cset -f -y 8 0x3d 0x6F 0xAA
i2cset -f -y 8 0x3d 0x6e 0xAA
i2cset -f -y 8 0x3d 0x6F 0xAA
i2cset -f -y 8 0x3d 0x4c 0x24
i2cset -f -y 8 0x3d 0x6e 0xAA
i2cset -f -y 8 0x3d 0x6F 0xAA
i2cset -f -y 8 0x3d 0x6e 0xAA
i2cset -f -y 8 0x3d 0x6F 0xAA
i2cset -f -y 8 0x3d 0x10 0x91
i2cset -f -y 8 0x3d 0x19 0x0A
i2cset -f -y 8 0x3d 0x1A 0xD7
i2cset -f -y 8 0x3d 0x1B 0xBA
i2cset -f -y 8 0x3d 0x1C 0x71
i2cset -f -y 8 0x3d 0x18 0x01
i2cset -f -y 8 0x3d 0x33 0x03
i2cset -f -y 8 0x3d 0x33 0x03
i2cset -f -y 8 0x3d 0x20 0x0C
i2cset -f -y 8 0x18 0x02 0x73
i2cset -f -y 8 0x18 0x0e 0x1e
i2cset -f -y 8 0x18 0x0d 0xe1
i2cset -f -y 8 0x19 0x02 0x73
i2cset -f -y 8 0x19 0x0e 0x1e
i2cset -f -y 8 0x19 0x0d 0xe1
i2cset -f -y 8 0x20 0x02 0x73
i2cset -f -y 8 0x20 0x0e 0x1e
i2cset -f -y 8 0x20 0x0d 0xe1
i2cset -f -y 8 0x21 0x02 0x73
i2cset -f -y 8 0x21 0x0e 0x1e
i2cset -f -y 8 0x21 0x0d 0xe1