This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 116
Part Number: DS110DF111
Hi Sir,
Our application is support 1.25 Gbps (1G SFP) and 10.3125 Gbps (10G SFP+).
some question about the register setting.
1. From datasheet page 21 (table 9), i know the default datarates are Group 0 = 1.25 Gbps and Group 1 = 10.3125 Gbps. (i guess the 00 means 10.3125 Gbps, but how about 01,10 and 11? )
2. and also i follow page 22 (table 13 and 14), to Calculate Group 0 and Group 1 Register 0X60-0X64. But the function still can't work.(the setting as below, any wrong please let me know)
(The 1.25Gbps setting is difference at e2e, the value is 0x60 =0x00 and 0x61 =0xB2, but why?)
3. Could you also descript about 9.8304 Gbps, why the Register 0X64 =0XFF?
4. When we use the default setting. the 1Gbps link is unstable, sometimes could get 1G link up status, but 10G always no work and CDR is unlocked...
BTW, What data should we provide for parameter adjustment?
Hi, see below my inputs to the questions.
See below table for standard rates based on channel register 0x2F values.
Table. Standards-Based Modes Register Settings
STANDARDS
DATA RATES (Gbps)
VCO FREQUENCIES (GHz)
DIVIDER RATIOS
REGISTER 0x2F VALUE (hex)
Ethernet
1.25, 10.3125
10.0, 10.3125
1, 8
0x06
Fibre-Channel
2.125, 4.25, 8.5, 10.51875
8.5, 10.51875
1, 2, 4
0x16
Infiniband
2.5, 5, 10
10.0
0x26
SDH/SONET
2.48832, 9.95328
9.5328
1, 4
0x56
PROP1a
8.25
1
0x76
PROP1b
8.5
0x86
Interlaken 2
10.3125
0xC6
SFF-8431
9.95328
0xD6
You may use the TI SigCon Architect GUI CDR tab to calculate the manual mode registers (0x60 - 0x64) values for you for a given data rate. However I would expect the values from datasheet table 12 to work.
https://www.ti.com/tool/SIGCONARCHITECT
If you are to set CDR for 1.25Gbps rate via channel registers 0x60 thru 0x64 my recommendation would be the following.
4. When we use the default setting. the 1Gbps link is unstable, sometimes could get 1G link up status, but 10G always no work and CDR is unlocked. BTW, What data should we provide for parameter adjustment?
Cordially,
Rodrigo Natal
In reply to Rodrigo Natal:
1. How to generate the PRBS pattern? by "SigCon Architect" tool?
If yes, please also provide the SOP.
2. Attached the setting.(it is default setting). default.cfg
so far
3. The 1G SFP link up and ping function is ok, but maybe still need fine tune parameters after provide the PRBS pattern.
4. 10G SFP+ only get link up information, but ping function is fail, we must fine tune the parameters.
thanks!
In reply to stanley wang:
Hi, see my inputs below.
Table. Register Writes to Enable PRBS Generator
STEP
SHARED/CHANNEL REGISTER SET
OPERATION
REGISTER ADDRESS [HEX]
REGISTER VALUE [HEX]
WRITE MASK [HEX]
COMMENT
Channel
Write
09
20
Override Output Multiplexer
Select.
2
1E
80
E0
Turn on serializer (ser_en=1).
3
10
Power-up PRBS Generator.
4
30
00
08
Reset PRBS Clock.
5
Power-up PRBS Clock.
6
02
03
Select PRBS9 pattern. Select PRBS31 pattern.
7
0D
Enable PRBS Clock triggering on Div/Clock so that the eye diagram is viewable. Disabling results in Pattern Cycle triggering.
HSSC Applications Engineer