This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002: Cable length

Part Number: TUSB1002

Hi Team,

May I ask how long could TUSB1002 support between the host and Receptacle when using the standard USB 3.0 cable? Could it support 3.6m in car?

If I only use one TUSB1002 between host and receptacle, does customer need to put it closed to host or closed to receptacle?

  • Hi Amelie,

    You will want to look at TUSB1002A, more specifically It is hard to say if this device can support this specific cable without knowing more about the cable qualilty, layout (trace length) between Host and TUSB1002A and whether or not this s a captive cable? In good conditions TUSB1002A can support such a cable but performance will vary with the items previously listed. 

    You will want to  have the redriver close to the receptacle.