hello
we are starting a design and we want to include TCA 9517 ( or TCA 9803) as a level shifter for I2c bus.
in one of the use cases we will have VCC1 = 3.3v and VCC2 = 1.8v
in other use case we will have VCC1=VCC2=3.3v (the system will go a full reset between the two caes)
there might even be a case where VCC1=VCC2=1.8v
so I have two questions:
1. is it o.k to use the shifter with both sides have same VCC
2. can the master (direction of the clock signal) be on both sides in this case?
thanks
Gil