This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS-485 Compatibility Between 3.3V-supply and 5V-supply Devices

Expert 3240 points

Replies: 15

Views: 18345

Recently, a designer asked, "Do you have an app note that explains why 3.3V and 5V 485 chips can operate on the same system?" 

Here is a short explanation of why you can mix and match RS-485 devices that use different supplies.

            The RS-485 standard (TIA-485-A) specifies the voltages and currents needed on the differential bus lines to ensure any compliant transceivers can communicate with each other.  The drivers must be capable of sourcing a 1.5V signal (either A > B +1.5V, or B > A +1.5V) into a standard load, and the receivers must be able to discriminate a differential signal as small as 200 mV (+ or -).  All of the original RS-485 transceivers used 5V supplies, which then allows for 3.5V of “headroom” for the driver circuits.  Newer designs for transceivers which operate with 3.3V supplies require more efficient driver stages, in order to develop 1.5V differential output signals.  

 

            On the receiver side, the allowable common-mode voltage range is from -7V to +12V according to the standard, which comes from adding 7V on either side of the original 0V and 5V power rails.  In order to discriminate a 200 mV differential signal on top of a 12V offset, the differential receivers first attenuate the input signals in order to bring the range within the linear region of the input stages.  For example, with 5V rails, a 4:1 attenuation through resistor dividers would “shrink” the 12V common-mode offset to 3V, which should be within the linear range of the input stage.  At the same time, the differential signal is also attenuated, so internally the receiver’s comparator stage would need a sensitivity of 50 mV in order to detect an external differential signal of 200 mV.  For devices with 3.3V supply, the attenuation must be slightly higher, for example a 6:1 attenuation would reduce a 12V common-mode offset to 2V; this will also require more sensitivity (about 33 mV) at the receiver comparator.

 

            These differences between devices with 5V supply and 3.3V supply account for the typically higher price for 3.3V transceivers compared to 5V transceivers; the output stages require larger transistors and the receiver stages require more accurate and sensitive circuit designs.  Texas Instruments used a variety of advanced process technologies and innovative circuit designs to develop RS-485 transceivers that fully comply with the RS-485 standard, whether the supply voltage is 3.3V or 5V.

-- Clark Kinnaird

15 Replies

  • In reply to Sheng Wang:

    Hi Sheng,

    Yes, it is OK for 3.3-V and 5-V RS-485 transceivers to share a common bus.

    Max
  • In reply to Sheng Wang:

    Hi Sheng,


    You are correct that you can connect a 3.3V transceiver and 5V transceiver together on the same network. Both types of transceivers are designed to drive a minimum Vod of 1.5V across a 54 ohm load so they can operate together.

    Regards,

    Michael Peffers

    Industrial Interface Applications

    Analog Wire: Get Connected

  • In reply to Michael Peffers:

    Thanks a lot, Max and Michael.

    Further considering, in the following two scenarios, is it still OK to directly connect both 3.3V transceiver and 5V transceiver?
    1/ Both transceivers have full failsafe feature
    2/ Need biasing resistors to handle open/idle bus (In this case, milliamphere level current will add on the resistor due to difference between 5V and 3.3V power) .

    Regards
    Sheng
  • In reply to Sheng Wang:

    HI Sheng,

    The answer to both questions is yes. Failsafe biasing weakly biases both types of parts to something around Vcc/2 so when these networks are combined, whether they are internal or external to the device, the Vcc/2 point will move to something between the two (i.e. 2V). There can be some differential offset as well depending on the biasing scheme and this is OK for 485 since the minimum input receiver threshold is 200mV.

    Please let me know if you have further questions?

    Regards,

    Michael Peffers

    Industrial Interface Applications

    Analog Wire: Get Connected

  • In reply to Michael Peffers:

    Thanks, Michael,

    I believe I got the perfect answers/support from you (and Max, Clark). I have no more questions on this.

    Regards

    Sheng

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.