This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 37
Part Number: DS90LV049
Dear Technical Support Team,
I have two questions about DS90LV049.
① Absolute maximum ratings
Is it possible to apply signal within following absolute max ranges when the power supply voltage is not applied to the DS90LV049?
LVDS input voltage -0.3V to +3.9VLVDS output voltage -0.3V to +3.9V② ESD withstand voltage
Are all pins effective flowing ESD spec?
HBM: ≧7kV, MM, 0Ω, 200pF ≧250V
Best Regards,
ttd
Hi ttd,
1. That should be okay - the datasheet does not specify that voltage on these pins is dependent on the supply voltage.
2. Yes
Regards,
I.K.