Can I use twisted pair cable or coaxial cable? Do you have any special requirements for the type of cable?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use twisted pair cable or coaxial cable? Do you have any special requirements for the type of cable?
Hello Zhang,
You can use either STP or coax for the 954-936. Usually, for ADAS applications, most customers use coax configuration and send power over the coax cable using DACAR 302 & 462. The requirements for the cable is to make sure you match the characteristic impedance, so 50 ohms for coax and 100 ohm differential for STP. Also, the entire channel must meet our channel specifications for the limits of the return loss and insertion loss parameters.
Thanks,
Sally