This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 78
Part Number: TCA9509
I have a customer with an I2C application in which either end of the bus wants to be 5V signaling but in between it needs to be 1.8V.
Gregory Duperon Part Number: TCA9509 I have a customer with an I2C application in which either end of the bus wants to be 5V signaling but in between it needs to be 1.8V. Can two A ports of a TCA9517at 1.8V be tied together while each of their B ports at 5V? [Bobby] Yes, as long as the B sides are not in contact with another I2C buffer on the static voltage offset side. Can the A port of a TCA9517 at 1.8V be tied to the A port of a TCA9509 also at 1.8V or would one need to swap out the TCA9509? [Bobby] TCA9509 has its offset set on the A side so A side of TCA9509 to A side of TCA9517 is okay. Would something completely than what is described above me better? [Bobby] What you have looks like it will work.