This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 71
Part Number: TPS65987EVM
HiWhen trying to import configuration settings from the EVM, into the Application customization tool, I get the following Exception
-------------------------------
Exception Encountered during I2C Test Read:*** ERROR in FTDI call (I2C_DeviceWrite), status: 2
<type 'exceptions.Exception'>
Traceback (most recent call last):
File "dialogWindow.pyc", line 7638, in test_read
File "device_rw.pyc", line 715, in read_reg
File "hw_interface.pyc", line 408, in hw_i2c_write_no_stop
File "ftdi.pyc", line 314, in ftdi_i2c_write
Exception
I2C adress set to 000b on S4 (all three off)
I2C adress set to 0x20 in Import Configuration
All S1 switches are OnException Occurs when I hit the Test Read button.What could the cause and solution to this be?Thanks, Thomas
Turned out i2c address was 0x38, problem solved
In reply to Thomas Nilsson:
Hi Thomas,
Thank you for the update. Closing this thread
Regards,
Adam McGaffin