This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 68
Part Number: TPS65987EVM
Hi
I am trying to import settings from EVM into Application Configuration tool.
I setup project according to manual, Standard template and DFP. But the Application Config tool does not end up looking like in the manual. There's no Nr of Devices selection in the Device Initialization Chain, just Device 1. I also don't get any Port X Settings tabs, just Port settings. ANd when I try to import there are no selections for Devices or Ports to import settings into, just Global Device Settings Tab and SharedDevices Tab, and when I import to those, I don't see any difference.
Please Advice!
And if I instead of Standard or Advanced when setting up New Project select TIDA-050012 Source Board, then I get a Device 1 tab and can select Device 1 Port 1 when importing, but then an Exception occurs.
Exception Encountered during Import From Device:list index out of range
<type 'exceptions.IndexError'>
Traceback (most recent call last):
File "dialogWindow.pyc", line 7699, in import_config
IndexError: list index out of range
In reply to Thomas Nilsson:
Hello,
I've assigned this issue to the relevant expert who will get back to you shortly
Regards,
Adam McGaffin
Thomas,
Here are the answers to your questions:
Robert Almendarez
This is indeed a bug in the tool, caused when settings are not shared between devices. This only occurs when the "Share Settings Across All Devices" is unchecked and the user selects a Device + Port option instead of Global or Shared Settings in the Import Configuration from Device menu. You can avoid this entirely by using the Standard or Advanced templates.
This bug will be fixed in the next release of the tool, 6.1.2.