Dear Specialists,
Regarding SN65HVD75, my customer is encountering noise issue.
I would be grateful if you coule advise.
---
There is a phenomenon that RS485 communication becomes abnormal at a specific frequency that is conducted immunity (IEC64000-4-6).
(Some points between 10MHz and 30MHz)
I put a ferrite bead (120Ω at 100MHz.) in series with the differential lines (A,B) of RS485, but it was not so effective.
When I changed it to 1.8kΩ at 100MHz as a trial, it improved significantly.
Originally, how much value ferrite bead should be put in these A and B lines?
Also, is there any improvement method other than inserting ferrite bead?
If you have an application note, please provide it.
---
I appreciate your great help in advance.
Best regards,
Shinichi