This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 640
Part Number: DP83TD510E
All,
Excited to share that "DP83TD510E" SPE (Single Pair Ethernet ) PHY, based on new standard IEEE 802.3cg 10Base-T1L is ready for evaluation.
The PHY is designed to reach 1.2Km+ using single pair ethernet cable with a very low power dissipation of 45 mW.
For datasheet, EVMs, please refer to Product Page :
https://www.ti.com/product/DP83TD510E
Regards,Geet
.
In reply to Geet Modi:
Hi, I'm not sure if this is the correct forum to post questions. I've never setup a TI board before and need to configure the DP83TD510 and DP83822 combination as a MASTER (I believe that is the default config) and a SLAVE (I have two of each). The USB-2-MDIO tool won't connect. Is there a way to configure them using jumpers or such?
In reply to Wayne Hopkinson:
Please ignore my earlier post. I'm not having trouble with the relationship between the two boards. My issue is related to getting the DP83822 to link with PC via RJ45 connection.
Please open a new thread with details on your problem.