Hello expert,
My customer has some questions below.
1) Can SN65DSI86 support eDP 1.4? --> after checking with E2E, I found eDP 1.4 is okay for SN65DSI86 but without PSR feature. correct me if it's wrong.
2) They only use SN65DSI86 Front-End (MIPI-DSI) for single-channel (4-lane). Based on this connection,how high could eDP panel resolution reach?
3) They will use two eDP panels, spec is shown below. Could SN65DSI86 (Front-End – Single channel MIPI-DSI) support below panel spec?
- 1920 x 3(RGB) x 1080, 2-lane eDP1.2
- 1920 x 3(RGB) x 1080, 4-lane eDP1.4
Best regards,
Ann Lien