Hi
We are currently developing a board that uses 2 x I210-IS devices that are configured in SGMII mode and these are then connected to the DS15MB200 so that we can change the destination PHY for each device.
We have found that after a few days of successful tests sending packets, the SGMII RX interface (MUX to I210) seems to break permanently while the SGMII TX (I210 to MUX) seems to continue to work.
This suggests that the TI MUX is maybe driving the SGMII RX incorrectly.
1. Is there a reference schematic of the DS15MB200 being used as an SGMII MUX?
2. Is there a reference design that uses the DS15MB200 and the Intel I210-IS?
3. Can you suggest why the MUX is permanently breaking the SGMII interface? We have AC coupled the TX and RX lines.
4. We think that this may be related to the drive strength or VOD (Differential Output Voltage). Can you suggest a way to lower this so that the SGMII interface does not break?
Thank you