This is a related post to the post by Stephen Zinck, posted on May 18, 2020 at 3:13pm.
We are seeing the same phenomena in our SI sims, i.e. the differences in loading on TX_D0 & TX_D1 (GPIO_SGMII_IN model) versus the TX_CLK, TX_CTRL & TX_D(3:2) (GPI model) is causing skew across the Tx RGMII bus.
Does the timing parameter IOskew=0.35ns in Table 3 of snla243 include the skew caused by the differences in input loading or should we add the skew we're seeing in our SI sims to the IOskew=0.35ns specified in snla243?
Or perhaps is the input loading skew included in one of the other delay parameters specified in snla243 ?
Please advise, thanks,
-John