This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
MAX3232: Heating problem with RS232 side connected at startup.
Replies: 1
Views: 41
Part Number: MAX3232
MAX3232 is stop working after some days.
and I have one doubt regarding C3 connection. as per datasheet C3 can be connected to VCC or GND.
my Question is, in which condition we connect C3 to VCC and in which condition C3 connect to GND ?
Thanks...
Hi,
Either way MAX3232 should work. Connecting C3 to Vcc or GND generates the same output voltage. Please refer to this blog (equation 2) for the discussion.
Regards,
Hao