Other Parts Discussed in Thread: TEST2
Dear Team,
Thank you for your help so far.
We have now finally received the new revision of the PCB, and we have fixed a couple of bugs in the driver.
The support for the monitor we are using for testing has improved, but we can still observe issues with some of the modelines exposed by the monitor over EDID:
- blinking
- dead monitor
- monitor reports no signal
- monitor is active but no picture
Other modelines work just fine.
Q1) Is the link training to blame for this? Do you have any idea as to why some modelines work just fine and other modelines are problematic?
We have been testing other monitors as well, some monitor work (although, with the same problems listed above), and other monitors won't work at all, like we get a dead monitor no matter what resolution we are trying to set. I wonder if the problem with monitors that don't work at all is the ASSR Display Authentication method?
Bit 0 = ALTERNATE_SCRAMBER_RESET_ENABLE
Source sets to 1 to select the alternate scrambler reset.
Writes ignored if ALTERNATE_SCRAMBLER_RESET_CAPABLE=0
Power-on default value = 0"
Bit 0 = ALTERNATE_SCRAMBLER_RESET_CAPABLE
A setting of 1 indicates that this is an eDP device that can use the eDP alternate
scrambler reset value of FFFEh."