This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Issue in RGMII Tx communication between FPGA and PHY.

Part Number: DP83867IR

Hi 

Relating to this below issue;

Is there any issue to interface Xilinx Kintex ultrascale+ devices with DP86867IR with VDDIO voltage 1V8.

As per datasheet, the VOL(0.45V) and VIL(0.36V) values are not matching.

but as stated in above issue, VIL max =0.6V is ok. Anyone can please give a confirmation for the same?

Thanks in advance.