Hi.
Can the TPS65981 be used without an application in the attached SPI flash and just control over I2C?
The Flash Read Flow in the datasheet, along with the Memory Invalid Flow show the device presenting a SWD interface on the USB-C lines for programming the flash. Does it permanently remain in that state for programming or is it possible to change the interface to, for example, a downward facing port via register CMD1?
Thanks,
Steve